Hi!
We have two custom boards, one with 66AK2H12 and other with 66AK2H06. Both PCB's are identical with the exception of the SoC. 66AK2H12 works fine but have a problem with 66AK2H06 and especially with Cortex-A-15 processors. We can not get connected to the target with CCS(v6.0.1.00040), following error message appears:
arm_A15_0: Trouble Halting Target CPU: (Error -1323 @ 0x94D0) Device failed to enter debug/halt mode because pipeline is stalled. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.600.0)
This happens with both of 66AK2H06 arm processors, however we can connect all the 4 DSP C66xx cores fine.
This leads to the question is there something else different than number of processors with these SoC's?
br,
JV