Issue 1:
We are still investigating throughput issues we are observing on our investigation of sending packets over SRIO. As part of that investigation, we took the TI tput example provided in the pdk and ran on the evm in loopback mode in a big-endian implementation. From the results that we got we have a query in regards to the performance numbers reported by the TI example. I am picking one of the packet sizes from the type 11 investigation. i.e. 512 which has a PCyc of 4784 cycles per packet. So to achieve 1.25 Gbps the actual data throughput according to the results is 856Mbps which means 209030 packets being sent from one core to another in one second. Those 209030 packets took 209030 x 4784 cycles to be received which translates to 1Gcycles/second i.e. the entire processing capability of the core. So my question is how can one actually do anything with the packets to do some actual processing on the data if it is taking 1G just to transfer the data. Granted we will not be doing type 11 and relying on message responses to go back from the consumer to the producer core so the numbers to send a single packet maybe of the order of 50% of the previous one. I would expect the time it takes to receive the packets to be even more negligible so that one can actually process the data and not have roughly 50% of the cycles available just to receive the data. I am recopying that line (just below) from the results much further below.
[C66xx_0] 0 1 1.250 C-I-C Type-11 24 512 0 856.19 209030.09 1200000 No 4784 592 4082 110 5.74
Issue 2:
Additionally, on our multi-core application we have configured 8 cores, with one driver per port (3 ports) per core with one socket per core for TX and one driver per core for Rx as each queue requires a separate driver. In addition we have 5 sockets per core for receive so total 64 sockets across 8 cores.
We also have 16k descriptors available for SRIO with 2048 per core of which 648 on a test basis I have assigned for Tx and the remaining 1400 are spread over the 5 sockets for Rx. We put the 1400 descriptors into a rx free queue for each core and make use of starvation queues where we drop on starvation.
In a given 10ms processing cycle, we are then creating a packet of size 500 bytes approx. and sending the packet 640 times by calling Srio_sockSend using a descriptor popped from the TX Free Q. We do that for 2 cores and send them both to a single core on another chip via an SRIO switch. We are able to see the statistics of the number of bytes received on various ports of the switch which are each connected to a DSP chip. On the Rx, We make a call to the driver function Srio_rxCompletionIsr in polled mode which gives us a count of the number of descriptors in the rxCompletion queue. We then receive all the packets in a given 10ms on the rx dsp by calling Srio_sockRecv on all the sockets will there are no more packets on the sockets and we then essentially discard them and do no further processing with them for now. What we are seeing is that we are not receiving in the driver all the packets we are expecting in any given 10ms window. This we are able to determine by keeping a running count of the rx completion queue i.e. Qmss_getQueueEntryCount(ptr_srioDrvInst->rxCompletionQueue). However, when we look at the statistics from the SRIO switch, we can see that the packets have been sent to the destination chip, but it appears that the hardware is dropping some of these packets and so not all the packets get pushed onto the Rx completion queue (general purpose queue). We should not be seeing any starvation on the Rx free queue because we have 1400 descriptors, and any given 10ms, we are expecting 1280 packets and hence 1280 descriptors should be used. I played around with the number of packets we send from the two cores and 500 from each core works without seeing any drops but when I tried 520 it did not.
[C66xx_0] ********************************
[C66xx_0] *********** CONSUMER ***********
[C66xx_0] ********************************
[C66xx_0] WARNING: Please ensure that the CONSUMER is executing before running the PRODUCER!!
[C66xx_0] Debug: Waiting for module reset...
[C66xx_0] Debug: Waiting for module local reset...
[C66xx_0] Debug: Waiting for SRIO ports to be operational...
[C66xx_0] Debug: SRIO port 0 is operational.
[C66xx_0] Debug: SRIO port 1 is operational.
[C66xx_0] Debug: SRIO port 2 is operational.
[C66xx_0] Debug: SRIO port 3 is operational.
[C66xx_0] Debug: Lanes status shows lanes formed as four 1x ports
[C66xx_0] Debug: AppConfig Tx Queue: 0x2a0 Flow Id: 0
[C66xx_0] Debug: SRIO Driver Instance 0x@00861540 has been created
[C66xx_0] Debug: Running test in polled mode.
[C66xx_0] Debug: SRIO Driver handle 0x861540.
[C66xx_0]
[C66xx_0]
[C66xx_1] ********************************
[C66xx_1] *********** PRODUCER ***********
[C66xx_1] ********************************
[C66xx_1] WARNING: Please ensure that the CONSUMER is executing before running the PRODUCER!!
[C66xx_1] Debug(Core 1): Waiting for SRIO to be initialized.
[C66xx_1] Debug: AppConfig Tx Queue: 0x2a1 Flow Id: 1
[C66xx_1] Debug: SRIO Driver Instance 0x@00861450 has been created
[C66xx_1] Debug: Running test in polled mode.
[C66xx_1] Debug: SRIO Driver handle 0x861450.
[C66xx_1]
[C66xx_1]
[C66xx_1] Latency: (Type-11, 1.250GBaud, 1X, tab delimited)
[C66xx_1] Core Lanes Speed Conn MsgType PktSize NumPkts MnLCycs AgLCycs MxLCycs
[C66xx_1] 1 1 1.250 C-I-C Type-11 16 100 2344 2376 2447
[C66xx_1] 1 1 1.250 C-I-C Type-11 32 100 2528 2581 2621
[C66xx_1] 1 1 1.250 C-I-C Type-11 64 100 2951 2988 3055
[C66xx_1] 1 1 1.250 C-I-C Type-11 128 100 3746 3810 3922
[C66xx_1] 1 1 1.250 C-I-C Type-11 256 100 5439 5477 5570
[C66xx_1] 1 1 1.250 C-I-C Type-11 512 100 7484 7562 7643
[C66xx_1] 1 1 1.250 C-I-C Type-11 1024 100 11948 12031 12150
[C66xx_1] 1 1 1.250 C-I-C Type-11 2048 100 22340 22428 22534
[C66xx_1] 1 1 1.250 C-I-C Type-11 4096 100 41188 41319 41480
[C66xx_1]
[C66xx_0] Throughput: (RX side, Type-11, 1.250GBaud, 1X, tab delimited)
[C66xx_0] Core Lanes Speed Conn MsgType OHBytes PktSize Pacing Thruput PktsSec. NumPkts PktLoss AgPCycs AgLCycs AgICycs AgOCycs Seconds
[C66xx_0] 0 1 1.250 C-I-C Type-11 24 16 0 173.91 1358695.63 6800000 No 736 593 33 110 5.01
[C66xx_0] 0 1 1.250 C-I-C Type-11 24 32 0 348.30 1360544.25 6800000 No 735 589 36 110 5.00
[C66xx_0] 0 1 1.250 C-I-C Type-11 24 64 0 609.52 1190476.25 6000000 No 840 595 135 110 5.04
[C66xx_0] 0 1 1.250 C-I-C Type-11 24 128 0 754.61 736919.69 3600000 No 1357 594 653 110 4.89
[C66xx_0] 0 1 1.250 C-I-C Type-11 24 256 0 856.19 418060.19 2200000 No 2392 595 1687 110 5.26
[C66xx_0] 0 1 1.250 C-I-C Type-11 24 512 0 856.19 209030.09 1200000 No 4784 592 4082 110 5.74
[C66xx_0] 0 1 1.250 C-I-C Type-11 24 1024 0 856.10 104504.13 600000 No 9569 593 8866 110 5.74
[C66xx_0] 0 1 1.250 C-I-C Type-11 24 2048 0 856.05 52249.33 400000 No 19139 594 18435 110 7.66
[C66xx_0] 0 1 1.250 C-I-C Type-11 24 4096 0 856.05 26124.67 200000 No 38278 592 37576 110 7.66
[C66xx_0]
[C66xx_1] Throughput: (TX side, Type-11, 1.250GBaud, 1X, tab delimited)
[C66xx_1] Core Lanes Speed Conn MsgType OHBytes PktSize Pacing Thruput PktsSec. NumPkts PktLoss AgPCycs AgLCycs AgICycs AgOCycs Seconds
[C66xx_1] 1 1 1.250 C-I-C Type-11 24 16 228 173.91 1358695.63 6800000 No 736 135 584 17 5.01
[C66xx_1] 1 1 1.250 C-I-C Type-11 24 32 228 348.30 1360544.25 6800000 No 735 135 583 17 5.00
[C66xx_1] 1 1 1.250 C-I-C Type-11 24 64 0 609.52 1190476.25 6000000 No 840 135 688 17 5.04
[C66xx_1] 1 1 1.250 C-I-C Type-11 24 128 0 754.61 736919.69 3600000 No 1357 135 1205 17 4.89
[C66xx_1] 1 1 1.250 C-I-C Type-11 24 256 0 856.19 418060.19 2200000 No 2392 135 2240 17 5.26
[C66xx_1] 1 1 1.250 C-I-C Type-11 24 512 0 856.19 209030.09 1200000 No 4784 135 4632 17 5.74
[C66xx_1] 1 1 1.250 C-I-C Type-11 24 1024 0 856.10 104504.13 600000 No 9569 135 9417 17 5.74
[C66xx_1] 1 1 1.250 C-I-C Type-11 24 2048 0 856.14 52254.79 400000 No 19137 135 18985 17 7.66
[C66xx_1] 1 1 1.250 C-I-C Type-11 24 4096 0 856.19 26128.76 200000 No 38272 135 38120 17 7.65
[C66xx_1]