Hello
We're trying to run multiple channels of MPEG2 to H.264 transcodes using sv04, MCSDK video v2.2.0.45 on DSPC8681.
I can run multiple encode channels on the same chip. But, multiple decodes don't run on the same chip.
For example, I'm using cores 0, 1, 2, 3 & 4, 5, 6, 7 for encodes for two inputs. But, when I use 8 & 9 for MPEG2 decodes, it doesn't work. It works ok if I use 8 & 16.
I noticed that the changes to enable concurrent encodes on the same chip were integrated starting from SDK v2.2. Can you please point me to the changes that I need to make to enable multiple decodes as well? Is there a patch?
Thank you.