Hi
I tried to execute the test_rel_ce66le_CE66LE_LE_ELF CCS project on XEVMK2EX and found perfectly working. We also created a new project and followed all settings in CCS for including ECU library to the same. This project also worked with perfect outputs. However we tried same to create a SYSBIOS project and observing input and output of Echo canceller as same. No cancellation is observed as output, same time the exact input file will be regenerated.
i) Kindly request support for the reason behind the generation of same input file as echo canceller output and moreover it will happen only when i use a SYSBIOS.
ii) only difference is SYSBIOS; i add Volib Package through SYSBIOS .cfg available products window anyway the project build is success without any errors.
Thanks & Regards,