Hi, I am using c6608 TI DSP to communicate with another SoC through the SRIO transfer. When I am doing a write operation, it is successful whereas when I do a read operation it fails with the transfer completion code being 3.
Can someone kindly explain the scenarios in which the completion code 3 is returned from the "GetLSUCompletionCode" function. That is, in LSU_STATUS register, the field Completion Code is set to 3 at the end of read transaction.
However, for write operation, "GetLSUCompletionCode" function returns the Completion code field as 0, which means transfer is complete without any errors.
Kindly help.
Best Regards,
Vaishnavi