Hello!
I have application for both cores c6657. I can run both cores simultaneously in debug session using group cores in CCSv5.
How to run both cores simultaneouly in standalone during booting from nand flash? I use TMDSEVMC6657.
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello!
I have application for both cores c6657. I can run both cores simultaneously in debug session using group cores in CCSv5.
How to run both cores simultaneouly in standalone during booting from nand flash? I use TMDSEVMC6657.
Thank you.
Hi, Rajasekaran.
Thank you for your answer, but I still did not understand how to build image in MAD utils.
I try to build example from "Demo walkthrough". I try step 1 - "Image Preparation" (Prelinker bypass mode demo). I use command: build_example_msys.sh c6657 little static, but it is no results.
My build_example_msys.sh file contains the following:
#!/bin/bash
#Build script to be invoked from BASH shell to build MAD loader example applications
if [ "$1" == "" ] ; then
echo "Device not specified"
echo "Usage: $0 C6678|C6670|C6657 big|little [static|relocatable]"
exit
fi
if [ "$3" == "static" ] ; then
mode="static"
libmode="static"
else
mode="relocatable"
libmode="shared"
fi
export C_DIR='"C:/ti/cgt_c6000_7.4.12"'
export PATH=$PATH:/c/ti/cgt_c6000_7.4.12/bin:$PATH
mkdir -p bin/$1/$endian
#Build for device $1
make -C shlibs/build clean all DEVICE=$1 ENDIAN=$2 MODE=$libmode
make -C app_1/build clean all DEVICE=$1 ENDIAN=$2 MODE=$mode
make -C app_2/build clean all DEVICE=$1 ENDIAN=$2 MODE=$mode
I use mcsdk_2_01_01_04 and windows 8.1.
How to do step 1 - Image Preparation?