We have an EVM2KH board with a 2 GB DDR3-1333 SO DIMM. According to the Keystone DDR3 memory controller manual (SPRUGV8D), the performance counter time register (PERF_CNT_TIM) increments at half the DDR3 memory clock speed. I see that the register increases at a rate of 409.8 MHz. This is not what I expect: with DDR3-1333 memory, I expect an I/O clock of 667 MHz, and thus PERF_CNT_TIM to increase at a rate of 333 MHz. How fast is the memory, and what bandwidth should I expect?
Thanks, John