Hello all,
I want to use IPC/MessageQ for C6678 cores. I have a different .out for each core. I can successfully imp;lement MEssageQ/IPC between cores 0 and 1, but when I added another core (core2), they never sync...I am using ipc_attach() from core 0 to cores 1/2...I have the MSM broken into 3 sections: IPC, MASTER, SLAVE...Do I need to break the SLAVE section into 2...one for core 1 and one for core 2...or the linker/etc will assign different memories to core 1 and 2?...the plan is to implement other cores too.
Regards,
Murad