Hi All,
As per the section 3.2.2 "Boot Table" of guide sprugy5(DSP bootloader guide),the boot table format should be
like below
(1) 32-bit header record indicating where the bootloader should branch after it has completed copying the data.
(2) For each initialized section:
– 32-bit section byte count
– 32-bit section address (destination address for the copy)
– The data to be copied
(3) A 32-bit termination record (0x00000000)
I understand that it is Boot Table format for single application image.
But if we want to load different images on different cores of DSP in case of TCI6638K2K,
then what should be the format of Boot Table and how RBL will know that which portion of
Boot Table should be loaded to which core.
Thanks & Regards,
Chandan