XEVMK2EX-K2E How many users Ethernet ports on card (I see two, but seems like there are 4)
How would I use the ethernet ports that are NOT the RJ-45 ports. I want to use the board standalone
Thanks
Bruce
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
XEVMK2EX-K2E How many users Ethernet ports on card (I see two, but seems like there are 4)
How would I use the ethernet ports that are NOT the RJ-45 ports. I want to use the board standalone
Thanks
Bruce
Is this
IS the :
Hi,
Yes, Rear-transition Module – Break-out Card (RTM-BOCRT) is available.
www.mistralsolutions.com/.../rtm-break-card-keystone-ii-evm
For more information, refer mistral solutions website.
Thanks,
Pleae go to
and look at the right side of the web page for the button "Click Here To Buy Now"
Rex