In the documentation, there is a reference to a T! 14-pin and 20-pin header for emulator support. The 14-pin header lacks all of the advanced trace / EMU pins except for EMU0 and EMU1. The 20 pin connection adds EMU2,3 & 4.
Question: What specific emulation or debugging features are not available when using the 14-pin or the 20-pin headers? Also, where is additional documentation on the 14-pin header. The SPRU655i document doesn't appear to have a pin out for the 14-pin header.
Thank you.