Hi,
I want to convert the EDMA based CSL to EDMA with SYS/BIOS .
give me an indication please.
Sincerely,
Zakaria.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to convert the EDMA based CSL to EDMA with SYS/BIOS .
give me an indication please.
Sincerely,
Zakaria.
Hi Zakaria,
Thanks for your post.
There are EDMA based SYS/BIOS examples under EDMA_LLD of MCSDK 2.0 folder which has test/demo code to demonstrate the EDMA3 driver functionality and it does EDMA3 mem-to-mem data copy testcase, EDMA3 ping-pong buffers based data copy test case on BIOS6. The examples can be found in the path below:
~\ti\mcsdk_2_01_02_06\edma3_lld_02_11_05_02\examples\edma3_driver\evm6678\sample_app
To program the EDMA3 using LLD,
http://processors.wiki.ti.com/index.php/Programming_the_EDMA3_using_the_Low-Level_Driver_%28LLD%29
http://processors.wiki.ti.com/images/5/5e/EDMA3_LLD.pdf
Likewise, you also have CSL based EDMA examples at the below loaction:
~\ti\mcsdk_2_01_02_06\pdk_C6678_1_1_2_6\packages\ti\csl\example\edma\edma_test.c
The above is the EDMA example test code uses the EDMA CSL functional layer for the c6678 device. You can build it for other targets (C6670, C6657 ) too through copying the above EDMA test source code into a new empty CCS project and link the functional CSL EDMA library (file name : ti.csl.ae66 ) by adding the directory to the library search path to the project properties->File Search Path. Then you can build this EDMA example in CCS and run without any issues.
http://processors.wiki.ti.com/index.php/CSL#Chip_Support_Library_for_C6670
Thanks & regards,
Sivaraj K
----------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
----------------------------------------------------------------------------------------------------------