Hello,
I am working on TCI 6670 EVM. I am using CPRI 4X link for AIF2 configuration. I am able to configure the AIF2 for 20 MHZ lte bandwidth and 10 MHz bandwidth in seperate run. But my requirement is to change the system bandwidth on the fly. For this I have reconfigured the following parameters:
1. DBMX settings for protocol decoder/encoder common setup.
2. FRM_MSG_TC for Protocol decoder/encoder link setup.
Beside these I am disabling the DMA channels associated with the cpri link and after reconfiguration i am enabling them back.
I have checked for errors from AIF2 but i am not getting any error after reconfiguration. But AIF2 loopback data is not passed after reconfigurations. Am i missing something. Should I need to reconfigure some more parameters for this?
Is there any document where I can read about the AIF2 parameters which can be reconfigured on the fly?
Regards,
Naveen