Chip: TMS320C6678
DSP 1 and DSP 2 establish a connection for sending data from DSP 1 to DSP 2 (a specified address: 0x833FFF00). (Chip 1 multicore boot, on removing the interrupts of core 1- 7, Chip 2 responds to the connection with the Chip 1 and receives data)
After the program run (corresponding LED lights), connect the two chips with emulator to view the data stored in the address.
When data is written correctly on Chip 2, the data viewed through Chip 1 is also correct; if data written to Chip 2 is wrong, data stored in the address viewed through chip 1 keeps changing.
May I ask what is the reason for this situation and how to solve this?
Thank you!