In the SRIO user guide (SPRUGW1B) section 2.3.11.1 the descriptions of the operation of the LOCAL_DIS bit and how to set it does not agree with the flow chart in figure 2-30 or the bit description in Table 3-18. The description says 1 means Rx packets are discarded. The table says 0 means packets are discarded. The description says if it =1 and PEREN=1, do a RESTORE, the figure says don't do a RESTORE.
What is the real description of this bit?
How should it be handled?
If is is discarding packets, does that mean that say, a DirectIO NREAD will not get a response? (Could this explain why I'm not seeing the NREAD response even though the FPGA is sending it?)
Thanks
Mike