Hi,
I have few doubts regarding I2C EEPROM booting and IBL
1. In I2C EEPROM booting readme.txt, it is given that writing .dat/.bin at 0x51, but I am able to boot keeping switch settings as
4 3 2 1
SW-3 1 0 1 1
SW-4 0 0 0 0
SW-5 0 0 0 0
SW-6 0 0 0 0
But SW-5[4] has to be 1 to boot from 0x51. How it is booting from 0x51 when I kept SW-5[4] (GPIO 11) as 0.
2. Can I2C EEPROM can be booted from 0x50?
3. Can I2C EEPROM can be booted from 0x51?
4. Can IBL be loaded in 0x50?
5. I am working on 6678 EVM Rev 3.0 and silicon rev 2.0. I created dat file for led.out using SPI NOR BOOTING steps and change the switch settings, I was able to see the led blinking. But when I load the multicore image processing demo(default) .bin file through the same procedure and change the switch settings, I am unable to see the result. But when I booted the image through SPI NOR OVER I2C EEPROM using IBL, I am able to see the result. If DDR3 initializations are there in the code, is IBL must (SPI NOR OVER I2C EEPROM)?. How I can boot the same image without using IBL, directly from SPI NOR?.