Hi,
I checked out
git.ti.com/.../92fa7f53f1f3f03296f8ffb14bdf1baefab83368
(Release 2015.1) as a baseline to build u-boot for 66AK2H12.
My custom board has 32-bit DDR3A and 32-bit DDR3B interfaces (no ECC).
SPRABX7 "Keystone II DDR3 Initialization" tells that PHY registers DX4GCR .. DX8GCR bit 0 need to be cleared. I tried to find those registers from the source tree, with no success.
1. What is the general procedure to adjust u-boot to fit custom board's DDR3 settings ?
2. Are there available any examples of 32-bit DDR3 for KS2 u-boot ?
3. The project is initialized with
make k2hk_evm_defconfig
and then the source files are edited. Is this a proper way to achieve target?
BR, -Topi