Hello all,
This post continues previous post:
e2e.ti.com/.../407402
I have modified project "Hello world" from
mcsdk_2_01_02_06\tools\boot_loader\examples\pcie\
to run this example on all cores in the L2SRAM
but Core1...Core7 did not start.
On previous post I have got answer:
"it does not support L2SRAM, Better to use DDR memory"
Could somebody explain:
- why this example does not work in L2SRAM?
- what necessary to do to force them work just in L2SRAM?
(it very necessary me with the performance reason)
I used:
Code Composer Studio 5.2.1.00018
mcsdk_2_01_02_06
MDSEVM6678L/MDXEVMPCI board
OS - Debian7, Ubuntu10.04
Best regards,
========================================================
P.S. I did not mark previuos post as "answered",
may be it was marked with the page's resources.