I have a question regarding the RapidIO (SRIO) and McBSP.
We have a new product under development that will use a high speed 14 bit A/D device with an LVDS output running at 910 Mbps with double data rate clock and frame clock outputs (500 MHz bandwith). The A/D will run continuously, but we will capture the data in 1k blocks at particular intervals.
We would like to use the TMS320C6657 in this application, however we don't think it will work using a direct connection. I've never used the SRIO or McBSP TI interfaces before, but I thought maybe they'll be suitable (might require a level translation?). However, after studying the specs we don't believe they are suitable for this continuous data stream.
At this point we're leaning towards the TigerSharc because it has the Link Ports which are perfect for capturing the data directly. Our first choice is still TI (as always) so before we go this route I want to make sure I've understood the high speed serial interface specs correctly. I believe RapidIO is a packet based methodology and not suited to a raw continous data stream and McBSP is too slow.
My question is: Can the TMS320C6657 be directly interfaced with a 500MHz DDR LVDS output and/or does TI have an alternative DSP that will work?