Hi,
We are currently trying to integrate the TCI6636K2H into our product architecture. One thing that is not entirely clear is what is the minimum number of input clocks that must be in place and active to allow the processor to bootload. Ideally with would like to hardwire these clocks and then have the processor itself configure the remainder. Section 3.6 of this document
http://www.ti.com/lit/an/sprabv0/sprabv0.pdf
provides some information but it is not clear which clocks would be mandatory to allow the SPI interface to the NOR flash to function and hence (I assume) the bootloader to be invoked. If anyone could point me to the appropriate document(s) or who could provide guidance based on their own experience, it would be appreciated.
Martin