hello all;
i am working on a project in whitch i need to get the connected components from a binary image . and i need a simple code exemple . because the project given by TI in the vlib_c66x_3_2_0_2 is very complicated .
thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello all;
i am working on a project in whitch i need to get the connected components from a binary image . and i need a simple code exemple . because the project given by TI in the vlib_c66x_3_2_0_2 is very complicated .
thank you.
Capitaine,
The test code available at present is the simplest we have, and it is simply initializing the input and representing the output. The actual library functions are only three function calls. Can you please let us know which part of the example code does not make sense to you? Thank you.
Sudhakar