Hello again.
Still working with simple project hua evm from here
And i'm still having troubles. Project requires to load the evmc6670l.gel file to work, with performing the global_default_setup to initialize the memory. I need to initialize the memory, without using the .gel file and while not changing the jumpers configuration.
I'm using the pdk_C6670_1_1_2_6, bios_6_33_06_50, ndk_2_21_02_43 and xdctools_3_23_04_60. Also i'm using c6000 compiler and Texas Instruments XDS100v1 USB Emulator with TMS320C6670 device for initial load.
Evaluation board is TMS320c6670l