Hi,
I have a question about C6670 VCP2 status register.
The question is about VCP2 Status Register(VCPSTAT0) bit[1]"RUN".
This bit[1]"RUN" description is as follows:
=============================
RUN:VCP running status bit
0 = VCP is not running
1 = VCP is running
=============================
Does this bit change to "1" immediately after calling VCP2_start(hVcp2)? and does the status stay in "1" until VCP2 outputs the decoded result?
VCP2_start() is API which defined in CSL.
VCP2_start() will set Start commad to VCP2 Execution Register(VCPEXE).
From VCP_start() description, it will affect to VCP2_VCPSTAT0_RUN=1.
So, I understood that setting Start Command to VCPEXE, VCPSTAT0.RUN will change to 1(running).
But is there a delay until VCPSTAT0.RUN change to "1" after Start Command?
best regards,
g.f.