Hello all,
The example mcsdk_2_01_02_06\tools\boot_loader\examples\pcie\pcieboot_helloworld
wokrs well under CCS when program is located in DDR or MSM, but
Core1-Core7 do not wake up when program is located in L2SRAM.
Could somebody give the example where Core0 wakes up Core1-Core7
and the same program's code is located in the corresponding CorePak's L2SRAM ?
Thank you a priori,
I used MDSEVM6678L+MDXEVMPCI boards, CCS 5.2.1.00018, mcsdk_2_01_02_06.
Best regards,
Marek