Hello again.
I'm using the 2.21.02.43 NDK and 2.01.02.06 MCSDK with an client example.
I want to send and recieve the raw ethernet packet, using only the C instructions, but i can't find any appropriate function, that could help me. Also, i can't watch port i should listen to, to intercept those packets. I've not changed the "evmc6670 client" example, but i want to add the "send" and "recieve" functions.