Hi,
I am using EVM6670 with CCS6. When I use the gel file in NO BOOT mode, Global default setup in evm6670l.gel is running on Target connect. But when I put the EVM in SRIO boot mode I have to run the gel scripts manually through CCS menu. We want to test a custom board which is in SRIO boot mode.
1. Is there a way to run the gel scripts on target connect in SRIO mode like No boot mode ? This helps us to configure the PLL in gel scripts.
2. What is the exact difference in No Boot and SRIO Boot modes for gel file execution ?
Thanks
Hari