Hi,
I am currently working on the TMS320TCI6614 board and encountering a unique problem. I have connected the board to a Ubuntu PC running Ubuntu 14.04 64bit via the Ethernet cable and to another PC running windows via the 560v2 USB emulator. The DSP cores are accessed through CCS running on windows machine and the ARM is accessed through the terminal of the Ubuntu machine.
The problem is that when code for the DSP is loaded via CCS the ARM already up and processing exits and doesn't turn on till the board is switched off and on again thereby removing the code on the DSP side.
I want to run the DSP as well as the ARM simultaneously can someone suggest a workaround.
Urgently required.
Thanks
Raunak