Hi All,
Use the 6678 EVM board has created a board.
JTAG connection, normally write programs to IBL files(EEPROM51.BIN) and SPI NOR memory.
However, should the SPI boot. DDR3 memory is operating normally.
If you read the GPIO value is 0x980B is read. But I read the DEVSTAT register the value 0xFFFF is read.
Why does the same? The accompanying diagram.
It did not put an FPGA in the EVM board. John does the problem is with the Reset or Power Sqeuence?
Thanks,