Hi,
AIF module does not send LOS and RAI bits when LOS occurs on RM side. RRU reads these two bits as ZERO.
Is there any enable bits to send those values to the RRU?
Thanks,
Mustafa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
AIF module does not send LOS and RAI bits when LOS occurs on RM side. RRU reads these two bits as ZERO.
Is there any enable bits to send those values to the RRU?
Thanks,
Mustafa
Yes, LOS and RAI information is passed from RM to TM, but to pass it back out you must enable it in TM. Please see the registers described in sections 7.5.3 and 8.4. You also may want to take a look at RM Configuration register 2 (see table 8-22).
Hi,
Thanks for your answer, I have another question.
What should we set the following three register?
1. num_los_det
2. sync_t
3. frame_sync_t
Their current values are 10, 21,21, and with these values, RM SYNC State is ST0. when I set `num_los_det` to 65000. RM SYNC State transits to ST1. After ST! RM does not transit to ST2 because we cannot receive consecutive valid bytes even when I set sync_t to 1.
What could be the reasons of not getting consecutive valid bytes on RM side?
Thanks,
Mustafa