It's nice to learn that in the new dsplib_c66x_3_4_0_0 you introduced the two functions,DSPF_sp_fftSPxSP_r2c() and DSPF_sp_ifftSPxSP_c2r(), to speed up FFT. However, there is little information on how to use them. I tried to run the fft and and ifft one after the other. I was expecting I can recover the fft input data. However, I could not. I wonder if you can point me to the right place to get more information. Thanks.