Hi to all
i try to rebuild 'ti.platform.evm6678l.ae66' library in pdk c6678 with the version of gcc (c6x-uclinux-gcc)
i have two solution:
S1 : rewrite makefile and rebuild library from source file (or edit exist makefile)
S2 : use ccs and edit project properties and replace CGT compiler to gcc
Q1:Do you know a better solution?
i start work on S2 but compiler and archiver options (FLAGS) is completely different and after removing all option (falgs) console report this:
....
../src/evm66x_i2c.c: line 1: /bin: is a directory
../src/evm66x_i2c.c: line 6: /bin: is a directory
../src/evm66x_i2c.c: line 7: ccsObjs.opt: command not found
../src/evm66x_i2c.c: line 8: ccsObjs.opt: command not found
../src/evm66x_i2c.c: line 9: ccsObjs.opt: command not found
......
that seem due to changing compiler
Q2: anybody can help me for this issue?
thanks
Ebi