Hi,
I have a question about C6678 PCIe RootComplex.
If C6678 PCIe is Rootcomplex, it will use BAR0 and BAR1.
BAR1 is used for 64-bit addressing mode.
I have a question about INBOUND address translation.
Is it possible to use 32-bit and 64-bit addresssing mode together for INBOUND address translation?
One more question.
C6678 (root complex) are communicating with FPGA(Endpoint) via PCIe. It seem that LinkUp is done, but can't Read/Write against memory space. The mapped memory space are all zero and doesn't update. Write access is also not availabe. In such case, does this mean that configuration of address translation is wrong? LinkUp is done(LTSSM[4:0]=0x11) so that I guess signal integrity is fine.
best regards,
g.f.