Hi,
When I run HEVC encoder (02.00.00.02 and 02.00.00.03) on 2 DSPs with multiple tiles it produces correct output.
But when I run it on 3 DSPs with 3 tiles or 4 DSPs with 4 tiles output has artifacts.
I use the same logic for 2, 3 and 4 DSP modes. Also I double checked that in\out buffers have the same addresses and contain the same data on all the DSPs.
Please see attached files: hevc_art.zip
Regards,
Andrey Lisnevich