Hello,
I have a question concerning the wiring of the unused addresses of DDR3 packages to a Keystone II.
We plan to use 2 packages of 1Gb on 16bits (2x 8 Meg x 16 bits x 8 banks).
We worry about the obsolescence of this memory. If in the future, we must mount a 2Gb (or 4Gb) as the 1Gb is no longer produced, the address A[13] (and A[15]/A[14] for a 4Gb and 8Gb) of this memory will not be NC. As it does not seem to be any pulldown internally, parasites could move the MSB of the address and make our design ineffective. That’s why we think to put the balls A[15..13] that are currently NC to GND if in a few years these balls become the MSB addresses of higher size memory components.
If a component memory size change is imposed, we do not intend to change neither our hardware design nor the soft into the Keystone II. So we would like to make the Keystone II "believe" that it still runs with 1Gb memories.
Question : What should we do with address signals A[15..13]? Can we simply connect it to GND (it seems dangerous to leave it NC)? Or should it absolutely be connected to the Keystone II? (we want to avoid this to simplify our layout).
Thank you in advance for your reply.