Not sure if this belongs here or in the Sys/Bios forum, so please excuse me if I am posting in the wrong place.
We are starting new development on the 66AK2L06 with Sys/Bios on the C66x. We will need to use I2C and SPI interfaces. I'd rather not reinvent wheel here, but I can't find any drivers for Initialization and the Read/Write from these devices. Hopefully I am just not looking in the right places. So, if they exist, could someone please point me to them? If not, then I guess I get the data sheet out and start writing code.
We will also have a Linux based process running on the ARMs. It has been discussed that since the peripherals are a shared resource, we could potentially use the ARMs running Linux to setup the I2C and SPI then have the DSP do the Read/Writes. That seems complicated to me, so for now I'd like to avoid that route if possible.