I encode the video with encoder version C66x_h264hpvenc_01_00_02_00_ELF_32bit, and I can use the sample test application.
When the resolution is 1920x1080,it can work well,but when it is 4096x3840,the application failed at creation.
It says I just have to change the parameters width, height and provide enough buffers.
I want to know the buffer needs when the resolution changed,how should I change the buffer size?
Thank you!