Hi,
This is just a quick conformation about the assumption for using power consumption spread sheet.
The numbers are calculated by using lower end of nominal CVDD voltage. For example, for 1400Mhz device, the nominal CVDD voltage is 0.95-1.15V, and the spread sheet uses 0.95 for the calculation.
Our understanding is this spread sheet would be used to calculate *max* power/current consumption in device point of view under provided conditions.
Here is the related document :
And it says:
The data found in this document and in the accompanying spreadsheet were measured from devices at the maximum end of the power consumption range for production devices.
Considering this, using higher end of CVDD for the calculation seems to be more likely consequence. Do you have any comments on this ? In fact, my customer is asking me the same question.
Best Regards,
Naoki