Hello everyone,
I'am working with OpenMP 2.x project on TMS320C6670. Seems I managed to overcome challenges to create, build and run the project with emulator. For correct DDR3 operation I initialize the memory with a GEL file.
Now I need to boot the device through the Ethernet. Before that I have created 2 stage boot loader. 1st stage initialize the DDR3 and then jumps to ROMBOOT_REENTRY_ADDRESS, so i can now boot with my application image. But when I'am trying to use an OpenMP image of the project instead of non-OMP image m application boot successfully, but not working.
Do I need to use some additional tools like MAD or whatever to boot OpenMP applications?
Best Regards,
Pavlo!