Hi
I want use spi nor flash boot mode on my 6678 custom board. In this board, I don’t use DDR memory and I’ll face some problem because of ignoring this memory. In the evaluation board I programmed spi nor flash successfully through using “eeprom51.bin” and now I want load my bin file on spi nor flash. As I know, I must load “eeprom51.bin” on eeprom and my bin file on nor flash. I changed the following line in source file “eepromwriter.c” for using MSMCSRAM memory instead of DDR.
#define WRITE_DATA_ADDRESS 0x0c000000
After that I load “eeprom51.bin” on my board’s eeprom but I faced the following error and I don’t know how can I fix this. Do you know??
[C66xx_0] EEPROM Writer Utility Version 01.00.00.05
Writing 52072 bytes from DSP memory address 0x0c000000 to EEPROM bus address 0x0051 starting from device address 0x0000 ...
Returned platform error number is 4
EEPROM write failed