We are currently debugging a 6678 core crash issue on our system and need some information from the TI documentation which seems to be missing. Referring to the latest version available, section 3.8.9.1 Interrupt status decode register, can you help providing the missing information of bit # 19 in the register shown below ? I suspect this is related to DIO AMU functional block, if so can you point to the right documentation manual corresponding to this block?
We are seeing this bit set.
http://www.ti.com/lit/ug/sprugw1b/sprugw1b.pdf