I would like allocate MSMC SRAM memory for descriptors.
Maybe you could point on some samples in SDK ?
I see several possibility but do not know proper way of doing this.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I would like allocate MSMC SRAM memory for descriptors.
Maybe you could point on some samples in SDK ?
I see several possibility but do not know proper way of doing this.
Welcome to the TI E2E forum. I hope you will find many good answers here and in the TI.com documents and in the TI Wiki Pages (for processor issues). Be sure to search those for helpful information and to browse for the questions others may have asked on similar topics (e2e.ti.com). Please read all the links below my signature.
We will get back to you on the above query shortly. Thank you for your patience.
Ran-
Apologies for bumping this thread, but could not find another post on this.
We're using c6678 and need to move PA descriptor queues/handles to MSMC SRAM from DDR3. We found that we can move everything in pa_mgmt.c and cppi_qmss_mgmt.c except for gHostDesc. If we place gHostDesc in MSMC packet I/O does not work correctly (no Rx packets received).
Is there something we're missing ? An assumption in other code that gHostDesc will be in DDR3 mem space ?
One note -- we did not move .cppiMemTX and .cppiMemRX, these are still in DDR3 mem (they are too large to move).
Thanks.
-Jeff
Signalogic
I may mention this before, or you already know that:
For 6678, the insert region function must be done in ascending order of the memory address (global memory if the address is in L2). This is due to the way the hardware translates between addresses and indexes of the descriptors. Make sure that you follow this statement.
Is this your case? update please
Best regards
Ran
Hi Ran-
Thanks for your reply.
>> For 6678, the insert region function must be done in ascending order of the
>> memory address
I can only find one Qmss_insertMemoryRegion() call, in cppi_qmss_mgmt.c:
memset (gHostDesc, 0, SIZE_HOST_DESC * NUM_HOST_DESC); memCfg.descBase = (UInt32 *) gHostDesc; memCfg.descSize = SIZE_HOST_DESC; memCfg.descNum = NUM_HOST_DESC; memCfg.manageDescFlag = Qmss_ManageDesc_MANAGE_DESCRIPTOR; memCfg.memRegion = Qmss_MemRegion_MEMORY_REGION0; memCfg.startIndex = 0; result = Qmss_insertMemoryRegion(&memCfg);
So if this one was DDR3 before, and now it is MSMC, then it should be ok unless there are one or more inserts being done in a TI lib that are not visible in the source. Could that be the case ?
Two additional notes:
1) I have seen a case where Rx packets got started, but stopped after 600 or so for each core (we're using UDP port filtering). Again, rebuilding with the only change moving gHostDesc back to DDR3 mem allows normal operation.
2) We did not move cppiMemTX and cppiMemRX, these are still in DDR3 mem. We could not make enough room in MSMC for these.
-Jeff