Hi Support,
Is there an EVK for TMS320C6655? Customer felt that the power consumption on TMS320C6657 EVK is high.
Is it possible to solder the TMS320C6655 onto the TMS320C6657 EVK?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Support,
Is there an EVK for TMS320C6655? Customer felt that the power consumption on TMS320C6657 EVK is high.
Is it possible to solder the TMS320C6655 onto the TMS320C6657 EVK?
Thanks.
Hi,
TMS320C6655 EVM is not available in market. Please use the TMS320C6657 EVM for your testing, TMS320C6657 have 2 DSP core and TMS320C6655 have single DSP core and both devices are same pin compatible.
Is it possible to solder the TMS320C6655 onto the TMS320C6657 EVK?
Hi Raja,
Is this confirmed by your hardware team?
In addition, may I know the use of TSIP. Its mentioned on the website: http://www.ti.com/product/TMS320C6655 but not in the datasheet: http://www.ti.com/lit/ds/symlink/tms320c6655.pdf
Thanks, Shaun.
Family of power-optimized, pin-compatible C665x DSPs comprising of single or dual C66x cores running at up to 1.25 GHz and delivering up to 80 GMACS/40 GFLOPS of fi xed- and floating-point performance.
• TMS320C6657 @ 1 GHz – 3.5 W
• TMS320C6655 @ 1 GHz – 2.5 W
• TMS320C6654 @ 850 MHz – <2 W
• Package: 21×21-mm FC-BGA