Hi everyone,
I am developping SPI driver with evaluation board "TMDSEVM6657". in this board, a FPGA communicates with the DSP with the SPI (CS1).
To begin, i have tested the SPI driver with loopback mode. And everything works well.
Now, i am trying to send message to FPGA with CS1 on SPI driver. But it doesn't work.
I'm not sure i have configure well the chips select 1 (registers SPIPC0, SPIDAT1 and SPIDEF)
After running, i have the error 0x11 in INTVEC0 register (error interrupt pending). This error can append when the frequency is too high. So i have changeg the frequency. But nothing changes.
So i took a oscilloscope to observe SPI signal (CLK, CS1, MISO, MOSI). The CLK signal seems good. But CS1 stays in high level. It nevers goes to low level.
Can anyone explain me clearly how to configure register to select CS1 ? (I have read many posts in this forum but i don't find the answer). If anyone could print me the SPI register after configuration, i would be grateful.
Thanks