Hello TI,
Here's the notes from my customer. I'm documenting in E2E but I think we will need a call set up.
Things are stuck right now. We have 3 issues at the moment:
1) The board will not boot from NAND flash, and apparently it never has. We have about one more day of probing to get some more definitive information than “won’t boot.” We intend to be able to see if the bus is hanging or if possibly uboot code being loaded is somehow corrupted. Immediate FAE support on this would be much appreciated.
2) We will be trying to get the codebase (which is only about 6 source files) moved over to CCS 6.2. This because CCS 5.4 is about 4 years old and is essentially obsolete, there have been dozens of bug fixes since then, and lastly my development system is Win10 which is not compatible with CCS 5. Right now we are having issues with compatibility of the old projects, including target config files, MCSDK, etc., and trying to get them converted to work with CCS 6. Are there utilities. Is there an App Note? FAE support on this would be much appreciated.
3) The EVM is a Model XTCIEVNK2X, Rev 2.0 and is not functioning (at least with CCS 6).
- I can talk to the serial port via FTDI/USB
- I can also talk to the JTAG/XDS200 via USB and the xds2xx_conf utility. I’ve updated it to Rev 1.0.0.8.
- On power up it is reporting “SOC Power Failure” which seems to be a known issue with Rev 2.0 hardware, along with a number of others (http://wfcache.advantech.com/www/support/TI-EVM/download/EVMK2HX_Rev2_0_Known_Issues.pdf)
- Basically, I need an EVM that will work, and I need it in short order. If we can’t work around this issue right away, any chance to get the latest Rev of EVM hardware (by Monday, when I leave town for some time and would like to take it with me to make progress while away)?
Please resolve what we can via email but for number 1 above that has been an on going issue where email back and forth hasn't worked.
Thanks,
Dan