Hi
I know that I can configure 6678 Ethernet module with 250MHz clock but in some project I must set Ethernet clock to 240MHz and I can not ping. Is there any way for working with 240MHz clock for Ethernet on 6678?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I know that I can configure 6678 Ethernet module with 250MHz clock but in some project I must set Ethernet clock to 240MHz and I can not ping. Is there any way for working with 240MHz clock for Ethernet on 6678?
In case of example, it doesn't matter. It will be ok if I can run client or helloworld project in 240MHz SGMII clock. I can get the IP and just not able to ping.
I set some changes in gel file such as:
#define PLL1_MULTIPLIER 8 (because my input DSP clock is 120MHz(not 100MHz))
SGMII_SERDES_CFGPLL = 0x00000051; (because my input DSP clock is 240MHz(not 312.5MHz))
Thank you so much.
Armin,
Please refer the C667x PLL Clocking spreadsheet which consists of all the peripheral clocking with their limitations.
8508.C667X_Clocking_Spreadsheet_V1.0_Sep2015.xlsm
Please note, this is preliminary version and yet to be released public.
Regards,
Senthil
Hi Senthikumar
I know that the ethernet can work with 156.25, 250 and 312.5MHz. My question is can ethernet work with 240MHz or not. If yes what changes I must do?
Armin,
The supported input frequencies are 156.25, 250 and 312.5 MHz. We do not support 240 MHz.
Regards,
Senthil