Hi experts,
I want to do local reset on C66x corepac. From C6678 datasheet i can see the description of local reset as below
MMR bit in LPSC controls C66x CorePac local reset. Used by watchdog
timers (in the event of a timeout) to reset C66x CorePac. Can also be
initiated by LRESET device pin. C66x CorePac memory system and slave
DMA port are still alive when C66x CorePac is in local reset. Provides a
local reset of the C66x CorePac, without destroying clock alignment or
memory contents. Does not initiate ROM boot process.
It says the memory system and SDMA port are still alive and it does not destroy clock alignment and memory contents.
My question is if the content in local L2 sram is destroyed in local reset?
Thank you.
Allen