Hi all,
I had used the WinDriver to create one PCIE demo project on Windows Host PC.
And the DSP project is using C:\ti\pdk_C6670_1_1_2_6\packages\ti\drv\exampleProjects\PCIE_exampleProject.
And now the Host PC PCIE demo project can read/write the DSP BAR1 memory space correctly.
Then I want to implement the Host PCIE DMA to access the DSP BAR1 memory space.
Do I need to modify something based on the project C:\ti\pdk_C6670_1_1_2_6\packages\ti\drv\exampleProjects\PCIE_exampleProject?
For simplicity, I do not use DSP's EDMA to access PC's memory through PCIE.
So I think I do not modify the C:\ti\pdk_C6670_1_1_2_6\packages\ti\drv\exampleProjects\PCIE_exampleProject to accommodate the Host PC. Am I right?
From the WinDriver view, its PCIE DMA demo codes need to write the device's registers like following picture.
Can anyone give some hints about this above?
Regards,
Feng