Hello.
I have two different *.out executable files for C6672 cores. The first exe file is "CORE0.out" and the second is "CORE1.out". All code sections in CORE0 should be located into L2-CORE0 memory. All CORE1 code sections should be loacated into L2-CORE1 memory.
I would like to boot all cores at one time. I can flash SPI-MEMORY and I am able to boot CORE0. I know that I can copy the "L2-image-core0" to "L2-memory-core1" but I do not want to solve it in that way. I need two independent threads/calc. There are no DDR3 memory devices on my board.
So far, I am thinking about two *.out files convertion and synthesis based on hex6x tools but I am not really sure is this right direction?
The best help for mi will be a script...
Best Regards
Pawel