Hi,
We are able boot our custom board using SPI NOR flash with out IBL.
Is the following statements are correct
1. The C6678 SPI boot support up to two images for selective booting.
2. The Parameter Table Index : Boot Sel [6-3] , can be used for selecting boot image offset byte address.
3. The offset byte address is 0xA000000 for image 1.
But where put this offset byte address in .bin file generation? . Is it in .rmd file?
can you share the process to boot using image-1 in SPI NOR. that is image 1 .bin generation.
Thanks in advance.
Ashok.M