I'm new to code composer, embedded programming and DSP. I have a C6678EVM with an XDS560v2 USB mezzanine emulation board attached and I cannot get the LED blink demo to work (or any demo to work for that matter... except for Hello World). I'm running CCSv6.1.3
I have poured through all the documentation, forums and read all the tips on what libraries to include, how to compile, what packages you need installed, etc... and I'm very stuck. I've have tried 3 different blink LED demos:
1) from the TI-RTOS workshop series (lab 4). I haven't managed to get this to compile
2 & 3) from the PDK_c667x_2_0_1 package where I have installed the example projects. This creates two LED demos. One called GPIO_LedBlink_C6678_EVM_c66xTestProject and the other called GPIO_LedBlink_C6678_EVM_c66xExampleProject (what is the difference between them?). I have gotten both of these to compile (without errors or warnings), but when they run, nothing happens. When I pause execution and step through the code they seem to be going through an Idle loop.
Which LED the on the EVM is supposed to blink?
How many cores do the demos run on? Should all cores be connected to the target? (I have tried connecting all 8 cores, running the .out file on just one core, and more or less every permutation of having the cores connected, running, paused, disconnected).
I'd appreciate any tips and help that can be provided.